config PM
	bool "Power Management support"
	depends on !IA64_HP_SIM
	---help---
	  "Power Management" means that parts of your computer are shut
	  off or put into a power conserving "sleep" mode if they are not
	  being used.  There are two competing standards for doing this: APM
	  and ACPI.  If you want to use either one, say Y here and then also
	  to the requisite support below.

	  Power Management is most important for battery powered laptop
	  computers; if you have a laptop, check out the Linux Laptop home
	  page on the WWW at <http://www.linux-on-laptops.com/> or
	  Tuxmobil - Linux on Mobile Computers at <http://www.tuxmobil.org/>
	  and the Battery Powered Linux mini-HOWTO, available from
	  <http://www.tldp.org/docs.html#howto>.

	  Note that, even if you say N here, Linux on the x86 architecture
	  will issue the hlt instruction if nothing is to be done, thereby
	  sending the processor to sleep and saving power.

config PM_DEBUG
	bool "Power Management Debug Support"
	depends on PM
	---help---
	This option enables various debugging support in the Power Management
	code. This is helpful when debugging and reporting PM bugs, like
	suspend support.

config PM_VERBOSE
	bool "Verbose Power Management debugging"
	depends on PM_DEBUG
	default n
	---help---
	This option enables verbose messages from the Power Management code.

config CAN_PM_TRACE
	def_bool y
	depends on PM_DEBUG && PM_SLEEP && EXPERIMENTAL

config PM_TRACE
	bool
	help
	  This enables code to save the last PM event point across
	  reboot. The architecture needs to support this, x86 for
	  example does by saving things in the RTC, see below.

	  The architecture specific code must provide the extern
	  functions from <linux/resume-trace.h> as well as the
	  <asm/resume-trace.h> header with a TRACE_RESUME() macro.

	  The way the information is presented is architecture-
	  dependent, x86 will print the information during a
	  late_initcall.

config PM_TRACE_RTC
	bool "Suspend/resume event tracing"
	depends on CAN_PM_TRACE
	depends on X86
	select PM_TRACE
	default n
	---help---
	This enables some cheesy code to save the last PM event point in the
	RTC across reboots, so that you can debug a machine that just hangs
	during suspend (or more commonly, during resume).

	To use this debugging feature you should attempt to suspend the
	machine, reboot it and then run

		dmesg -s 1000000 | grep 'hash matches'

	CAUTION: this option will cause your machine's real-time clock to be
	set to an invalid time after a resume.

config PM_SLEEP_SMP
	bool
	depends on SMP
	depends on ARCH_SUSPEND_POSSIBLE || ARCH_HIBERNATION_POSSIBLE
	depends on PM_SLEEP
	select HOTPLUG_CPU
	default y

config PM_SLEEP
	bool
	depends on SUSPEND || HIBERNATION || XEN_SAVE_RESTORE || HIBERNATION_ON_MEMORY
	default y

config SUSPEND
	bool "Suspend to RAM and standby"
	depends on PM && ARCH_SUSPEND_POSSIBLE
	default y
	---help---
	  Allow the system to enter sleep states in which main memory is
	  powered and thus its contents are preserved, such as the
	  suspend-to-RAM state (e.g. the ACPI S3 state).

config PM_TEST_SUSPEND
	bool "Test suspend/resume and wakealarm during bootup"
	depends on SUSPEND && PM_DEBUG && RTC_CLASS=y
	---help---
	This option will let you suspend your machine during bootup, and
	make it wake up a few seconds later using an RTC wakeup alarm.
	Enable this with a kernel parameter like "test_suspend=mem".

	You probably want to have your system's RTC driver statically
	linked, ensuring that it's available when this test runs.

config SUSPEND_FREEZER
	bool "Enable freezer for suspend to RAM/standby" \
		if ARCH_WANTS_FREEZER_CONTROL || BROKEN
	depends on SUSPEND
	default y
	help
	  This allows you to turn off the freezer for suspend. If this is
	  done, no tasks are frozen for suspend to RAM/standby.

	  Turning OFF this setting is NOT recommended! If in doubt, say Y.

config HIBERNATION_NVS
	bool

config HIBERNATION
	bool "Hibernation (aka 'suspend to disk')"
	depends on PM && SWAP && ARCH_HIBERNATION_POSSIBLE
	select HIBERNATION_NVS if HAS_IOMEM
	---help---
	  Enable the suspend to disk (STD) functionality, which is usually
	  called "hibernation" in user interfaces.  STD checkpoints the
	  system and powers it off; and restores that checkpoint on reboot.

	  You can suspend your machine with 'echo disk > /sys/power/state'
	  after placing resume=/dev/swappartition on the kernel command line
	  in your bootloader's configuration file.

	  Alternatively, you can use the additional userland tools available
	  from <http://suspend.sf.net>.

	  In principle it does not require ACPI or APM, although for example
	  ACPI will be used for the final steps when it is available.  One
	  of the reasons to use software suspend is that the firmware hooks
	  for suspend states like suspend-to-RAM (STR) often don't work very
	  well with Linux.

	  It creates an image which is saved in your active swap. Upon the next
	  boot, pass the 'resume=/dev/swappartition' argument to the kernel to
	  have it detect the saved image, restore memory state from it, and
	  continue to run as before. If you do not want the previous state to
	  be reloaded, then use the 'noresume' kernel command line argument.
	  Note, however, that fsck will be run on your filesystems and you will
	  need to run mkswap against the swap partition used for the suspend.

	  It also works with swap files to a limited extent (for details see
	  <file:Documentation/power/swsusp-and-swap-files.txt>).

	  Right now you may boot without resuming and resume later but in the
	  meantime you cannot use the swap partition(s)/file(s) involved in
	  suspending.  Also in this case you must not use the filesystems
	  that were mounted before the suspend.  In particular, you MUST NOT
	  MOUNT any journaled filesystems mounted before the suspend or they
	  will get corrupted in a nasty way.

	  For more information take a look at <file:Documentation/power/swsusp.txt>.

config PM_STD_PARTITION
	string "Default resume partition"
	depends on HIBERNATION
	default ""
	---help---
	  The default resume partition is the partition that the suspend-
	  to-disk implementation will look for a suspended disk image. 

	  The partition specified here will be different for almost every user. 
	  It should be a valid swap partition (at least for now) that is turned
	  on before suspending. 

	  The partition specified can be overridden by specifying:

		resume=/dev/<other device> 

	  which will set the resume partition to the device specified. 

	  Note there is currently not a way to specify which device to save the
	  suspended image to. It will simply pick the first available swap 
	  device.

config HIBERNATION_ON_MEMORY
	bool "Hibernation on memory"
	depends on PM
	select HIBERNATION
	---help---
	  Enable the hibernation on memory (HoM) functionality. This techniques
	  will put the memory in self-refresh and after that it will turn-off
	  the chip.

config HOM_TAG_VIRTUAL_ADDRESS
	hex "Hibernation on memory - Tag virtual addess"
	depends on HIBERNATION_ON_MEMORY
	depends on SUPERH32
	default "0x80001800"
	---help---
	  Set the Absolute Virtual Address where the Hibernation

config HOM_DEBUG
	bool "Hibernation on memory - Debug"
	depends on HIBERNATION_ON_MEMORY
	depends on SUPERH32
	default n
	---help---
	  This option enables the hom_printk function. This works
	  like a standard printk on the empty_zero_page.
	  It's used as a rudimental printk to debug.

config APM_EMULATION
	tristate "Advanced Power Management Emulation"
	depends on PM && SYS_SUPPORTS_APM_EMULATION
	help
	  APM is a BIOS specification for saving power using several different
	  techniques. This is mostly useful for battery powered laptops with
	  APM compliant BIOSes. If you say Y here, the system time will be
	  reset after a RESUME operation, the /proc/apm device will provide
	  battery status information, and user-space programs will receive
	  notification of APM "events" (e.g. battery status change).

	  In order to use APM, you will need supporting software. For location
	  and more information, read <file:Documentation/power/pm.txt> and the
	  Battery Powered Linux mini-HOWTO, available from
	  <http://www.tldp.org/docs.html#howto>.

	  This driver does not spin down disk drives (see the hdparm(8)
	  manpage ("man 8 hdparm") for that), and it doesn't turn off
	  VESA-compliant "green" monitors.

	  Generally, if you don't have a battery in your machine, there isn't
	  much point in using this driver and you should say N. If you get
	  random kernel OOPSes or reboots that don't seem to be related to
	  anything, try disabling/enabling this option (or disabling/enabling
	  APM in your BIOS).

config PM_RUNTIME
	bool "Run-time PM core functionality"
	depends on PM
	---help---
	  Enable functionality allowing I/O devices to be put into energy-saving
	  (low power) states at run time (or autosuspended) after a specified
	  period of inactivity and woken up in response to a hardware-generated
	  wake-up event or a driver's request.

	  Hardware support is generally required for this functionality to work
	  and the bus type drivers of the buses the devices are on are
	  responsible for the actual handling of the autosuspend requests and
	  wake-up events.