#
# Architectures that offer an FUNCTION_TRACER implementation should
#  select HAVE_FUNCTION_TRACER:
#

config USER_STACKTRACE_SUPPORT
	bool

config NOP_TRACER
	bool

config HAVE_FTRACE_NMI_ENTER
	bool
	help
	  See Documentation/trace/ftrace-implementation.txt

config HAVE_FUNCTION_TRACER
	bool
	help
	  See Documentation/trace/ftrace-implementation.txt

config HAVE_FUNCTION_GRAPH_TRACER
	bool
	help
	  See Documentation/trace/ftrace-implementation.txt

config HAVE_FUNCTION_GRAPH_FP_TEST
	bool
	help
	 An arch may pass in a unique value (frame pointer) to both the
	 entering and exiting of a function. On exit, the value is compared
	 and if it does not match, then it will panic the kernel.

config HAVE_FUNCTION_TRACE_MCOUNT_TEST
	bool
	help
	  See Documentation/trace/ftrace-implementation.txt

config HAVE_DYNAMIC_FTRACE
	bool
	help
	  See Documentation/trace/ftrace-implementation.txt

config HAVE_FTRACE_MCOUNT_RECORD
	bool
	help
	  See Documentation/trace/ftrace-implementation.txt

config HAVE_KPTRACE
	bool

config HAVE_HW_BRANCH_TRACER
	bool

config HAVE_SYSCALL_TRACEPOINTS
	bool
	help
	  See Documentation/trace/ftrace-implementation.txt

config TRACER_MAX_TRACE
	bool

config RING_BUFFER
	bool

config FTRACE_NMI_ENTER
       bool
       depends on HAVE_FTRACE_NMI_ENTER
       default y

config EVENT_TRACING
	select CONTEXT_SWITCH_TRACER
	bool

config CONTEXT_SWITCH_TRACER
	bool

config RING_BUFFER_ALLOW_SWAP
	bool
	help
	 Allow the use of ring_buffer_swap_cpu.
	 Adds a very slight overhead to tracing when enabled.

# All tracer options should select GENERIC_TRACER. For those options that are
# enabled by all tracers (context switch and event tracer) they select TRACING.
# This allows those options to appear when no other tracer is selected. But the
# options do not appear when something else selects it. We need the two options
# GENERIC_TRACER and TRACING to avoid circular dependencies to accomplish the
# hidding of the automatic options.

config TRACING
	bool
	select DEBUG_FS
	select RING_BUFFER
	select STACKTRACE if STACKTRACE_SUPPORT
	select TRACEPOINTS
	select NOP_TRACER
	select BINARY_PRINTF
	select EVENT_TRACING

config GENERIC_TRACER
	bool
	select TRACING

#
# Minimum requirements an architecture has to meet for us to
# be able to offer generic tracing facilities:
#
config TRACING_SUPPORT
	bool
	# PPC32 has no irqflags tracing support, but it can use most of the
	# tracers anyway, they were tested to build and work. Note that new
	# exceptions to this list aren't welcomed, better implement the
	# irqflags tracing for your architecture.
	depends on TRACE_IRQFLAGS_SUPPORT || PPC32
	depends on STACKTRACE_SUPPORT
	default y

if TRACING_SUPPORT

menuconfig FTRACE
	bool "Tracers"
	default y if DEBUG_KERNEL
	help
	 Enable the kernel tracing infrastructure.

if FTRACE

config FUNCTION_TRACER
	bool "Kernel Function Tracer"
	depends on HAVE_FUNCTION_TRACER
	select FRAME_POINTER
	select KALLSYMS
	select GENERIC_TRACER
	select CONTEXT_SWITCH_TRACER
	help
	  Enable the kernel to trace every kernel function. This is done
	  by using a compiler feature to insert a small, 5-byte No-Operation
	  instruction to the beginning of every kernel function, which NOP
	  sequence is then dynamically patched into a tracer call when
	  tracing is enabled by the administrator. If it's runtime disabled
	  (the bootup default), then the overhead of the instructions is very
	  small and not measurable even in micro-benchmarks.

config FUNCTION_GRAPH_TRACER
	bool "Kernel Function Graph Tracer"
	depends on HAVE_FUNCTION_GRAPH_TRACER
	depends on FUNCTION_TRACER
	depends on !X86_32 || !CC_OPTIMIZE_FOR_SIZE
	default y
	help
	  Enable the kernel to trace a function at both its return
	  and its entry.
	  Its first purpose is to trace the duration of functions and
	  draw a call graph for each thread with some information like
	  the return value. This is done by setting the current return 
	  address on the current task structure into a stack of calls.


config IRQSOFF_TRACER
	bool "Interrupts-off Latency Tracer"
	default n
	depends on TRACE_IRQFLAGS_SUPPORT
	depends on GENERIC_TIME
	select TRACE_IRQFLAGS
	select GENERIC_TRACER
	select TRACER_MAX_TRACE
	select RING_BUFFER_ALLOW_SWAP
	help
	  This option measures the time spent in irqs-off critical
	  sections, with microsecond accuracy.

	  The default measurement method is a maximum search, which is
	  disabled by default and can be runtime (re-)started
	  via:

	      echo 0 > /sys/kernel/debug/tracing/tracing_max_latency

	  (Note that kernel size and overhead increases with this option
	  enabled. This option and the preempt-off timing option can be
	  used together or separately.)

config PREEMPT_TRACER
	bool "Preemption-off Latency Tracer"
	default n
	depends on GENERIC_TIME
	depends on PREEMPT
	select GENERIC_TRACER
	select TRACER_MAX_TRACE
	select RING_BUFFER_ALLOW_SWAP
	help
	  This option measures the time spent in preemption off critical
	  sections, with microsecond accuracy.

	  The default measurement method is a maximum search, which is
	  disabled by default and can be runtime (re-)started
	  via:

	      echo 0 > /sys/kernel/debug/tracing/tracing_max_latency

	  (Note that kernel size and overhead increases with this option
	  enabled. This option and the irqs-off timing option can be
	  used together or separately.)

config SYSPROF_TRACER
	bool "Sysprof Tracer"
	depends on X86
	select GENERIC_TRACER
	select CONTEXT_SWITCH_TRACER
	help
	  This tracer provides the trace needed by the 'Sysprof' userspace
	  tool.

config SCHED_TRACER
	bool "Scheduling Latency Tracer"
	select GENERIC_TRACER
	select CONTEXT_SWITCH_TRACER
	select TRACER_MAX_TRACE
	help
	  This tracer tracks the latency of the highest priority task
	  to be scheduled in, starting from the point it has woken up.

config ENABLE_DEFAULT_TRACERS
	bool "Trace process context switches and events"
	depends on !GENERIC_TRACER
	select TRACING
	help
	  This tracer hooks to various trace points in the kernel
	  allowing the user to pick and choose which trace point they
	  want to trace. It also includes the sched_switch tracer plugin.

config FTRACE_SYSCALLS
	bool "Trace syscalls"
	depends on HAVE_SYSCALL_TRACEPOINTS
	select GENERIC_TRACER
	select KALLSYMS
	help
	  Basic tracer to catch the syscall entry and exit events.

config BOOT_TRACER
	bool "Trace boot initcalls"
	select GENERIC_TRACER
	select CONTEXT_SWITCH_TRACER
	help
	  This tracer helps developers to optimize boot times: it records
	  the timings of the initcalls and traces key events and the identity
	  of tasks that can cause boot delays, such as context-switches.

	  Its aim is to be parsed by the scripts/bootgraph.pl tool to
	  produce pretty graphics about boot inefficiencies, giving a visual
	  representation of the delays during initcalls - but the raw
	  /debug/tracing/trace text output is readable too.

	  You must pass in initcall_debug and ftrace=initcall to the kernel
	  command line to enable this on bootup.

config TRACE_BRANCH_PROFILING
	bool
	select GENERIC_TRACER

choice
	prompt "Branch Profiling"
	default BRANCH_PROFILE_NONE
	help
	 The branch profiling is a software profiler. It will add hooks
	 into the C conditionals to test which path a branch takes.

	 The likely/unlikely profiler only looks at the conditions that
	 are annotated with a likely or unlikely macro.

	 The "all branch" profiler will profile every if statement in the
	 kernel. This profiler will also enable the likely/unlikely
	 profiler as well.

	 Either of the above profilers add a bit of overhead to the system.
	 If unsure choose "No branch profiling".

config BRANCH_PROFILE_NONE
	bool "No branch profiling"
	help
	 No branch profiling. Branch profiling adds a bit of overhead.
	 Only enable it if you want to analyse the branching behavior.
	 Otherwise keep it disabled.

config PROFILE_ANNOTATED_BRANCHES
	bool "Trace likely/unlikely profiler"
	select TRACE_BRANCH_PROFILING
	help
	  This tracer profiles all the the likely and unlikely macros
	  in the kernel. It will display the results in:

	  /sys/kernel/debug/tracing/profile_annotated_branch

	  Note: this will add a significant overhead, only turn this
	  on if you need to profile the system's use of these macros.

config PROFILE_ALL_BRANCHES
	bool "Profile all if conditionals"
	select TRACE_BRANCH_PROFILING
	help
	  This tracer profiles all branch conditions. Every if ()
	  taken in the kernel is recorded whether it hit or miss.
	  The results will be displayed in:

	  /sys/kernel/debug/tracing/profile_branch

	  This option also enables the likely/unlikely profiler.

	  This configuration, when enabled, will impose a great overhead
	  on the system. This should only be enabled when the system
	  is to be analyzed
endchoice

config TRACING_BRANCHES
	bool
	help
	  Selected by tracers that will trace the likely and unlikely
	  conditions. This prevents the tracers themselves from being
	  profiled. Profiling the tracing infrastructure can only happen
	  when the likelys and unlikelys are not being traced.

config BRANCH_TRACER
	bool "Trace likely/unlikely instances"
	depends on TRACE_BRANCH_PROFILING
	select TRACING_BRANCHES
	help
	  This traces the events of likely and unlikely condition
	  calls in the kernel.  The difference between this and the
	  "Trace likely/unlikely profiler" is that this is not a
	  histogram of the callers, but actually places the calling
	  events into a running trace buffer to see when and where the
	  events happened, as well as their results.

	  Say N if unsure.

config POWER_TRACER
	bool "Trace power consumption behavior"
	depends on X86
	select GENERIC_TRACER
	help
	  This tracer helps developers to analyze and optimize the kernels
	  power management decisions, specifically the C-state and P-state
	  behavior.


config STACK_TRACER
	bool "Trace max stack"
	depends on HAVE_FUNCTION_TRACER
	select FUNCTION_TRACER
	select STACKTRACE
	select KALLSYMS
	help
	  This special tracer records the maximum stack footprint of the
	  kernel and displays it in /sys/kernel/debug/tracing/stack_trace.

	  This tracer works by hooking into every function call that the
	  kernel executes, and keeping a maximum stack depth value and
	  stack-trace saved.  If this is configured with DYNAMIC_FTRACE
	  then it will not have any overhead while the stack tracer
	  is disabled.

	  To enable the stack tracer on bootup, pass in 'stacktrace'
	  on the kernel command line.

	  The stack tracer can also be enabled or disabled via the
	  sysctl kernel.stack_tracer_enabled

	  Say N if unsure.

config HW_BRANCH_TRACER
	depends on HAVE_HW_BRANCH_TRACER
	bool "Trace hw branches"
	select GENERIC_TRACER
	help
	  This tracer records all branches on the system in a circular
	  buffer giving access to the last N branches for each cpu.

config KMEMTRACE
	bool "Trace SLAB allocations"
	select GENERIC_TRACER
	help
	  kmemtrace provides tracing for slab allocator functions, such as
	  kmalloc, kfree, kmem_cache_alloc, kmem_cache_free etc.. Collected
	  data is then fed to the userspace application in order to analyse
	  allocation hotspots, internal fragmentation and so on, making it
	  possible to see how well an allocator performs, as well as debug
	  and profile kernel code.

	  This requires an userspace application to use. See
	  Documentation/trace/kmemtrace.txt for more information.

	  Saying Y will make the kernel somewhat larger and slower. However,
	  if you disable kmemtrace at run-time or boot-time, the performance
	  impact is minimal (depending on the arch the kernel is built for).

	  If unsure, say N.

config WORKQUEUE_TRACER
	bool "Trace workqueues"
	select GENERIC_TRACER
	help
	  The workqueue tracer provides some statistical informations
          about each cpu workqueue thread such as the number of the
          works inserted and executed since their creation. It can help
          to evaluate the amount of work each of them have to perform.
          For example it can help a developer to decide whether he should
          choose a per cpu workqueue instead of a singlethreaded one.

config BLK_DEV_IO_TRACE
	bool "Support for tracing block io actions"
	depends on SYSFS
	depends on BLOCK
	select RELAY
	select DEBUG_FS
	select TRACEPOINTS
	select GENERIC_TRACER
	select STACKTRACE
	help
	  Say Y here if you want to be able to trace the block layer actions
	  on a given queue. Tracing allows you to see any traffic happening
	  on a block device queue. For more information (and the userspace
	  support tools needed), fetch the blktrace tools from:

	  git://git.kernel.dk/blktrace.git

	  Tracing also is possible using the ftrace interface, e.g.:

	    echo 1 > /sys/block/sda/sda1/trace/enable
	    echo blk > /sys/kernel/debug/tracing/current_tracer
	    cat /sys/kernel/debug/tracing/trace_pipe

	  If unsure, say N.

config DYNAMIC_FTRACE
	bool "enable/disable ftrace tracepoints dynamically"
	depends on FUNCTION_TRACER
	depends on HAVE_DYNAMIC_FTRACE
	default y
	help
         This option will modify all the calls to ftrace dynamically
	 (will patch them out of the binary image and replaces them
	 with a No-Op instruction) as they are called. A table is
	 created to dynamically enable them again.

	 This way a CONFIG_FUNCTION_TRACER kernel is slightly larger, but otherwise
	 has native performance as long as no tracing is active.

	 The changes to the code are done by a kernel thread that
	 wakes up once a second and checks to see if any ftrace calls
	 were made. If so, it runs stop_machine (stops all CPUS)
	 and modifies the code to jump over the call to ftrace.

config FUNCTION_PROFILER
	bool "Kernel function profiler"
	depends on FUNCTION_TRACER
	default n
	help
	 This option enables the kernel function profiler. A file is created
	 in debugfs called function_profile_enabled which defaults to zero.
	 When a 1 is echoed into this file profiling begins, and when a
	 zero is entered, profiling stops. A file in the trace_stats
	 directory called functions, that show the list of functions that
	 have been hit and their counters.

	 If in doubt, say N

config FTRACE_MCOUNT_RECORD
	def_bool y
	depends on DYNAMIC_FTRACE
	depends on HAVE_FTRACE_MCOUNT_RECORD

config FTRACE_SELFTEST
	bool

config FTRACE_STARTUP_TEST
	bool "Perform a startup test on ftrace"
	depends on GENERIC_TRACER
	select FTRACE_SELFTEST
	help
	  This option performs a series of startup tests on ftrace. On bootup
	  a series of tests are made to verify that the tracer is
	  functioning properly. It will do tests on all the configured
	  tracers of ftrace.

config EVENT_TRACE_TEST_SYSCALLS
	bool "Run selftest on syscall events"
	depends on FTRACE_STARTUP_TEST
	help
	 This option will also enable testing every syscall event.
	 It only enables the event and disables it and runs various loads
	 with the event enabled. This adds a bit more time for kernel boot
	 up since it runs this on every system call defined.

	 TBD - enable a way to actually call the syscalls as we test their
	       events

config MMIOTRACE
	bool "Memory mapped IO tracing"
	depends on HAVE_MMIOTRACE_SUPPORT && PCI
	select GENERIC_TRACER
	help
	  Mmiotrace traces Memory Mapped I/O access and is meant for
	  debugging and reverse engineering. It is called from the ioremap
	  implementation and works via page faults. Tracing is disabled by
	  default and can be enabled at run-time.

	  See Documentation/trace/mmiotrace.txt.
	  If you are not helping to develop drivers, say N.

config MMIOTRACE_TEST
	tristate "Test module for mmiotrace"
	depends on MMIOTRACE && m
	help
	  This is a dumb module for testing mmiotrace. It is very dangerous
	  as it will write garbage to IO memory starting at a given address.
	  However, it should be safe to use on e.g. unused portion of VRAM.

	  Say N, unless you absolutely know what you are doing.

config RING_BUFFER_BENCHMARK
	tristate "Ring buffer benchmark stress tester"
	depends on RING_BUFFER
	help
	  This option creates a test to stress the ring buffer and bench mark it.
	  It creates its own ring buffer such that it will not interfer with
	  any other users of the ring buffer (such as ftrace). It then creates
	  a producer and consumer that will run for 10 seconds and sleep for
	  10 seconds. Each interval it will print out the number of events
	  it recorded and give a rough estimate of how long each iteration took.

	  It does not disable interrupts or raise its priority, so it may be
	  affected by processes that are running.

	  If unsure, say N

endif # FTRACE

config KPTRACE
	tristate "KPTrace (EXPERIMENTAL)"
	depends on HAVE_KPTRACE
	select KPROBES
	select DEBUG_FS
	select RELAY
	select SYSFS
	select KALLSYMS
	help
	  KPTrace is a kprobes-based dynamic trace tool. It provides a full
	  set of optional pre-defined tracepoints, plus a simple way to add
	  and remove tracepoints at runtime.

config KPTRACE_SYNC
       bool "Trace synchronization events"
       depends on KPTRACE
       default n
       help
        For KPTrace to be able to trace synchonization events (for example
        mutex and semaphore usage), certain key functions like mutex_lock
        must not be inlined. This may adversely affect system performance,
        and so this option must be used with care.

endif # TRACING_SUPPORT