menuconfig SND_STM
	tristate "STMicroelectronics SoCs support"
	depends on SND
	depends on CPU_SUBTYPE_STX7100 || CPU_SUBTYPE_STX7105 || CPU_SUBTYPE_STX7111 || CPU_SUBTYPE_STX7141 || CPU_SUBTYPE_STX7200
	select STM_DMA
	select SND_PCM
	help
		Say Y here for ALSA support on the STMicroelectronics SoCs.

		This driver provides core functionality - you have to build
		(at least one) SoC-specific driver as well. Additionally, it is
		using dynamic device minor number allocation, so udev-like
		utility is required.

		It is recommended to have BPA2 enabled with dedicated
		partition defined, however it is not absolutely necessary.

		To compile this driver as a module, choose M here: the module
	 	will be called snd-stm.ko

config SND_STM_BPA2_PARTITION_NAME
	string "Name of BPA2 partition to allocate buffers from"
	depends on SND_STM
	depends on BPA2
	default "audio"
	help
		Define a name of BPA2 partition the driver should try to
		allocate from.

		If name is not given or given partition does not exist, driver
		will try to use "bigphysmem" partition or eventually
		preallocate some system memory using
		ALSA snd_pcm_lib_preallocate_pages_for_all() method.

		This value can be overridden by module parameter
		"bpa2_part=<name>" (or kernel command line parameter
		"snd-stm.bpa2_part=<name>", if driver is compiled into
		kernel).

config SND_STM_DEBUG_LEVEL
	int "Default debug verbosity level"
	depends on SND_STM
	depends on SND_DEBUG
	default 0
	help
		Defines debug verbosity level (bigger number equals more
		messages). This can be overridden using "debug=<n>" module
		parameter or "snd-stm.debug=<n>" kernel command line
		parameter. You can also change this value in runtime,
		using /sys/module/snd_stm/parameters/debug.

		There is also fine-grained debug verbosity control available -
		just put "#define DEBUG <n>" in debugged component _before_
		#including "common.h", or alter the value using sysfs file
		/sys/module/snd_stm/parameter/debug_component_name (or
		use module/kernel command line parameter ;-)...

config SND_STM_STX7100
	tristate "STx7100 and STx7109 support"
	depends on SND_STM
	default y if CPU_SUBTYPE_STX7100
	help
		Select this to get ALSA driver for STx7100 and STx7109 chips.

		If you compile this driver as a module, it will be
		called snd-stm-stx7100.ko

config SND_STM_STX7105
	tristate "STx7105 support"
	depends on SND_STM
	default y if CPU_SUBTYPE_STX7105
	help
		Select this to get ALSA driver for STx7105 chip.

		If you compile this driver as a module, it will be
		called snd-stm-stx7105.ko

config SND_STM_STX7111
	tristate "STx7111 support"
	depends on SND_STM
	default y if CPU_SUBTYPE_STX7111
	help
		Select this to get ALSA driver for STx7111 chip.

		If you compile this driver as a module, it will be
		called snd-stm-stx7111.ko

config SND_STM_STX7141
	tristate "STx7141 support"
	depends on SND_STM
	default y if CPU_SUBTYPE_STX7141
	help
		Select this to get ALSA driver for STx7141 chip.

		If you compile this driver as a module, it will be
		called snd-stm-stx7141.ko

config SND_STM_STX7200
	tristate "STx7200 support"
	depends on SND_STM
	default y if CPU_SUBTYPE_STX7200
	help
		Select this to get ALSA driver for STx7200 chip.

		If you compile this driver as a module, it will be
		called snd-stm-stx7111.ko

config SND_STM_CONV_DUMMY
	tristate "Dummy converter driver"
	depends on SND_STM
	help
		This provides dummy converter driver to configure
		digital audio interface format (I2S, Left-Justified,
		Right-Justified). See include/sound/stm.h for
		more information.

		If compiled as module, it will be called
		snd-stm-conv-dummy.ko.

config SND_STM_CONV_EPLD
	tristate "Generic EPLD-controlled converter driver"
	depends on SND_STM
	depends on SH_ST_EPLD
	help
		This provides generic driver for EPLD-controlled
		converters. See include/sound/stm.h for informations
		how to define EPLD offsets & values.

		If compiled as module, it will be called
		snd-stm-conv-epld.ko.

config SND_STM_CONV_GPIO
	tristate "Generic GPIO-controlled converter driver"
	depends on SND_STM
	help
		This provides generic driver for GPIO-controlled
		converters. See include/sound/stm.h for informations
		how to define GPIO line numbers.

		If compiled as module, it will be called
		snd-stm-conv-gpio.ko.

config SND_STM_CONV_I2C
	tristate "Generic I2C-controlled converter driver"
	depends on SND_STM && I2C
	help
		This provides generic driver for I2C-controlled
		converters. See include/sound/stm.h for informations
		how to define required I2C addresses & commands.

		If compiled as module, it will be called
		snd-stm-conv-i2c.ko.