Licenses for the BACnet Stack at SourceForge

This BACnet protocol stack implementation is specifically 
designed for the embedded BACnet appliance, using a GPL with 
exception license (like eCos), which means that any changes 
to the core code that are distributed must be made available
in accordance with section (3) of the GNU General Public License.
However, the BACnet library can be linked to proprietary code 
without the proprietary code becoming GPL.

The text of the GPL exception included in each source file 
is as follows:

    "As a special exception, if other files instantiate 
     templates or use macros or inline functions from 
     this file, or you compile this file and link it 
     with other works to produce a work based on this file, 
     this file does not by itself cause the resulting work 
     to be covered by the GNU General Public License. 
     However the source code for this file must still be 
     made available in accordance with section (3) of the 
     GNU General Public License."

Each file that is subject to the GPL uses the following text comment
at the top of the file:

/*####COPYRIGHTBEGIN####
 -------------------------------------------
 Copyright (C) 2005 Steve Karg

 This program is free software; you can redistribute it and/or
 modify it under the terms of the GNU General Public License
 as published by the Free Software Foundation; either version 2
 of the License, or (at your option) any later version.

 This program is distributed in the hope that it will be useful,
 but WITHOUT ANY WARRANTY; without even the implied warranty of
 MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 GNU General Public License for more details.

 You should have received a copy of the GNU General Public License
 along with this program; if not, write to:
 The Free Software Foundation, Inc.
 59 Temple Place - Suite 330
 Boston, MA  02111-1307, USA.

 As a special exception, if other files instantiate templates or
 use macros or inline functions from this file, or you compile
 this file and link it with other works to produce a work based
 on this file, this file does not by itself cause the resulting
 work to be covered by the GNU General Public License. However
 the source code for this file must still be made available in
 accordance with section (3) of the GNU General Public License.

 This exception does not invalidate any other reasons why a work
 based on this file might be covered by the GNU General Public
 License.
 -------------------------------------------
####COPYRIGHTEND####*/

The example and demo files are licensed using an MIT style 
license, officially called an Expat License by GNU, and is 
compatible with the GPL.  The files subject to this license 
include the following text comment at the top of the file:

/**************************************************************************
*
* Copyright (C) 2005 Steve Karg <skarg@users.sourceforge.net>
*
* Permission is hereby granted, free of charge, to any person obtaining
* a copy of this software and associated documentation files (the
* "Software"), to deal in the Software without restriction, including
* without limitation the rights to use, copy, modify, merge, publish,
* distribute, sublicense, and/or sell copies of the Software, and to
* permit persons to whom the Software is furnished to do so, subject to
* the following conditions:
*
* The above copyright notice and this permission notice shall be included
* in all copies or substantial portions of the Software.
*
* THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND,
* EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF
* MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT.
* IN NO EVENT SHALL THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY
* CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT,
* TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE
* SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE.
*
*********************************************************************/